Can not flash the board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can not flash the board

665 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Fri Feb 10 05:24:28 MST 2012
I am using LPCXPresso LPC1769 board. When I try to debug the board I can not flash it!!
IDE does not progress after 68% of progress:(
0 项奖励
回复
1 回复

655 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Sun Feb 12 18:44:49 MST 2012
I get that sometimes.   In my case, I have to make sure that the previous instance of the debugger is not running.   Sometimes it continues to run even when the debug window goes away.     To kill it, I unplug the USB cable.

I discovered this problem because I always run "Process Explorer" which is a free task manager from SysInternals, a devision of microsoft.     It is a much better task manager than the one that comes with Windows.      I will occassionally see two debuggers running.      When this happens, the newly launched debugger cannot get control of the LPCXpresso from the old one and it seems to wait forever.

Instead of unplugging the USB cable, you can also kill them using Process Explorer.

Hope this helps,
Pete.
0 项奖励
回复