CLOCK speed problem during debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLOCK speed problem during debug

1,066 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dr Whom on Thu Mar 18 06:23:41 MST 2010
Hello

I have a problem when running single wire debug through a J link and an LPC 1313

During debug mode with IAR, my Clock out is exactly 10 Mhz and outside the debug it is the expected 12 Mhz from Internal RC.

Anybody run into this already?
0 项奖励
回复
2 回复数

1,033 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dr Whom on Tue Mar 23 05:53:29 MST 2010

Quote: Dr Whom
Hello

I have a problem when running single wire debug through a J link and an LPC 1313

During debug mode with IAR, my Clock out is exactly 10 Mhz and outside the debug it is the expected 12 Mhz from Internal RC.

Anybody run into this already?



FYI

My problem was that my J-link needed to be set for 'Halt after bootloader'

If the bootloader does not run, it will not load the trim values for the internal RC to give you 12 Mhz
0 项奖励
回复

1,033 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Fri Mar 19 11:49:26 MST 2010
Hello,

I have not had that problem.
LPC1343 and CodeRed IDE.
0 项奖励
回复