CLKOUT Superimposed on 3.3v

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLKOUT Superimposed on 3.3v

779件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by deBoogle on Tue Oct 11 03:36:13 MST 2011
Hi Guys,
Can anybody offer a suggestion as to why the clkout signal is being superimposed onto 3.3v.

When I turn the pin back to an input (with mode set to inactive), it is being held at 3.3v, It should have no connections to 3v3 and I cannot see any shorts to 3v3 on the board?

Slightly puzzled!!!

deBoogle
0 件の賞賛
返信
2 返答(返信)

771件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by deBoogle on Tue Oct 11 05:25:44 MST 2011
Hi Zero,

This was my bad.  Had the clkout connected to a tri state bus that was configured in the opposite direction.

oops

thanks for looking in tho!!!

deBoogle
0 件の賞賛
返信

771件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Oct 11 05:00:45 MST 2011
Could suggest something if I would know which LPC we are talking about :confused:
Still LPC17xx ?

A piece of code could also be useful :)
0 件の賞賛
返信