C reference manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C reference manual

1,098件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dave3891 on Wed Jun 08 22:59:10 MST 2011
Does anyone have a gook link for a site or PDF of a reference manual for programming the LPCxpresso in C?

I know that the Red Code comes with examples, but I am looking for a reference / list for all the functions such as [SIZE=2][SIZE=3]GPIOSetDir, [/SIZE][SIZE=2][SIZE=3]enable_timer16, [SIZE=2][SIZE=3]GPIOInit, etc.[/SIZE][/SIZE][/SIZE][/SIZE][/SIZE]
[SIZE=2][SIZE=2][SIZE=3][SIZE=2][SIZE=3][/SIZE][/SIZE][/SIZE][/SIZE][/SIZE]
[SIZE=2][SIZE=2][SIZE=3][SIZE=2][SIZE=3]Thanks[/SIZE][/SIZE][/SIZE][/SIZE][/SIZE]
[SIZE=2][SIZE=2][SIZE=3][SIZE=2][SIZE=3]Dave[/SIZE]
[/SIZE][/SIZE][/SIZE][/SIZE]
0 件の賞賛
返信
3 返答(返信)

1,089件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Fri Jun 10 12:41:58 MST 2011
the lpc1xxx.h does not do much more than provide the symbols that are written down in the lpc1xxx user manual to the programmer as C defines.

As far as the other functions go, the functions in the CMS project are defined in the CMS specification by Arm and functions like GPIOSetDir, enable_timer etc are all specific to some example projects.

I agree with Zero: these functions were deprecated even before they were written. Do not assume that any of these function will do what you want them to.
There is no standard library to use the peripherals in the lpc1xxx but there always is the user manual telling you how to program these peripherals.

Rob
0 件の賞賛
返信

1,089件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dave3891 on Thu Jun 09 06:36:34 MST 2011
I tryed control-H and it does allow me to search for functions.

But I am looking for ALL of the functions that are avaliable for this chip and a description of what they do.
Something like a document of the lcp1xxx.h and other header files.

I looked in the getting started guide, but I could not find anything.

I must be looking in the wrong places or something?


Thanks
Dave
0 件の賞賛
返信

1,089件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jun 09 00:40:36 MST 2011
Isn't that a little bit old fashioned, a list of function that's outdated before it's written :confused:

If you are trying to find this functions in real LPCXpresso, CTRL-H is a good friend to find things like that somewhere in workspace[SIZE=3] :)[/SIZE][SIZE=2][SIZE=2][SIZE=3][SIZE=2][SIZE=3]
[/SIZE][/SIZE][/SIZE][/SIZE][/SIZE]
0 件の賞賛
返信