Build failing!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build failing!

1,278 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Thu Sep 02 06:25:30 MST 2010
This is weird! I haven't used the Code Red software for some time, and I'm now unable to build any programs. I'm using v3.4.6, and I get the following when I build any of the examples for the LPC1114 LPCXpresso:

*** Build of configuration Debug for project LPCXpresso1114_blinky ****

make all
m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x3F0000, m.State 0x10000
C:\NXP\lpcxpresso_3.4\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2400000>) in child, Win32 error 0
make: *** [src/blinky.o] Error 1

I also lose the USB connection to the LPCXpresso.

I've just received an LPC1343 LPCXpresso, and tried that first, which is when I got the problem, trying to build the examples for that.

I'm using Win7 x64. V3.4.6 always worked without any problems previously.
0 Kudos
Reply
4 Replies

1,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Thu Sep 02 08:36:38 MST 2010
3.50 seems OK, at any rate. I'll bear what you said in mind if the problem recurs with that.
0 Kudos
Reply

1,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 02 08:07:31 MST 2010
No it doesn't. This is a VERY VERY rare occurrence and we supply a new DLL to people who it affects. If you want to find out more, google for"  Couldn't reserve space for cygwin's heap"
0 Kudos
Reply

1,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Thu Sep 02 07:11:38 MST 2010
Thanks, that fixed the problem. I noticed that there is a new version 3.50, which I've just downloaded, which presumably includes that new dll.
0 Kudos
Reply

1,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 02 06:41:12 MST 2010
Looks like you are encountering a known, but very unusual to encounter, issue with msys. For more details, including how to avoid this, please see:

http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull

Regards,
CodeRedSupport.
0 Kudos
Reply