Bluetooth Stack (btstack) for LPC mcu (LPC1768,LPC4330,etc.)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth Stack (btstack) for LPC mcu (LPC1768,LPC4330,etc.)

1,931 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by legato on Sun Jun 09 19:20:02 MST 2013
Hello guys,

         Does someone here have done this? [COLOR=Red][SIZE=2][B]Integrating the bluetooth stack (btstack) in the MCU?[/B][/SIZE][/COLOR] Hope you could give me some helpful tips and links. I have also seen this example which is using msp430 but i would like to do it in LPX mcu's ..thanks
0 Kudos
Reply
3 Replies

1,608 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by legato on Tue Jun 11 03:26:02 MST 2013

Quote: capiman
Hello Legato,
can you write a bit what you want to do with the integrated Bluetooth stack?
Which feature/profiles do you want in detail?
Best regards,
Martin



Hello Martin,

     Thanks for your concern. We want to integrate a bluetooth stack for the bluetooth low energy of the PAN1323 module from panasonic which has the TI CC2564 chip. I saw the example and manual with the bluekitchen ([COLOR=Red][SIZE=2]https://code.google.com/p/btstack/wiki/EmbeddedSystems#Details[/SIZE][/COLOR]) but it is using the MSP430 mcu though it was together with the pan1323 module and Im having trouble undestanding it. I thought of porting the btstack they did to lpc mcu but really i could not move because im very unfamiliar with their guides like they use makefile and everything. I use LPCXpresso as my IDE. So basically I want to do like what blue kitchen with the MSP430 mcu but with our MCU which is the LPC4330 or LPC1768.

thanks


Quote: cfb
There are Bluetooth stack examples for the mbed (an LPC1768 development board) here:

http://mbed.org/users/va009039/code/BTstack/



hello cfb,

         Have you tried this one brother? how do you find it and does it act like the one example of bluekitchen. I will check this later though.. thanks
0 Kudos
Reply

1,608 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfb on Tue Jun 11 01:31:22 MST 2013
There are Bluetooth stack examples for the mbed (an LPC1768 development board) here:

http://mbed.org/users/va009039/code/BTstack/
0 Kudos
Reply

1,608 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Tue Jun 11 01:11:38 MST 2013
Hello Legato,
can you write a bit what you want to do with the integrated Bluetooth stack?
Which feature/profiles do you want in detail?
Best regards,
Martin
0 Kudos
Reply