Blinky compile error on win7 64bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Blinky compile error on win7 64bit

2,326 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by daffy1108 on Mon Apr 12 09:23:36 MST 2010
I need some help debugging install or setup problems.
I'm using my win7 64bit laptop and 3.3.3 version of the binaries.
When I try to compile with debug the "Blinky" test,
I got one error related to missing LPC11xx.h
so I searched under the c:/nxp subdirectories
and found that it was located under an examples directory
c:\nxp\lpcxpresso_3.3\Examples\LPC1000\LPC11xx\1114examples\CMSIS1pv30_LPC11xx\inc
I added this to the include directory paths.
Now I'm getting a different compile error "eabi/bin/ld.exe: cannot find -lCMSISv1p30_LPC11xx"

How to fix this error?

David


Building target: blinky.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -L"" -Xlinker -Map=blinky.map -mcpu=cortex-m0 -mthumb -T "lpcxpresso1114_blinky_Debug.ld" -o"blinky.axf"  ./src/blinky_main.o ./src/clkconfig.o ./src/cr_startup_lpc11.o ./src/gpio.o ./src/timer32.o   -lCMSISv1p30_LPC11xx
c:/nxp/lpcxpresso_3.3/tools/bin/../lib/gcc/arm-none-eabi/4.3.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -lCMSISv1p30_LPC11xx
collect2: ld returned 1 exit status
arm-none-eabi-gcc.exe: unrecognized option '-Map=blinky.map'
make: *** [blinky.axf] Error 1
0 Kudos
Reply
6 Replies

2,299 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Apr 13 00:04:25 MST 2010
It is probably not documented specifically, but you are the first (of thousands) to have reported this particular issue.

Anyway, I am glad you are now up and running.
0 Kudos
Reply

2,299 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by daffy1108 on Mon Apr 12 17:25:08 MST 2010
Ok.
After I imported all of the examples, I can compile successfully.
Are there instructions to import all of the files before compiling?
Did I miss some instructional videos or README?
David
0 Kudos
Reply

2,299 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 12 15:06:35 MST 2010
You have to import all of the examples and not just one. There are library projects in the examples bundle that blinky and others rely on. Cmsis is one such library
0 Kudos
Reply

2,297 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by daffy1108 on Mon Apr 12 14:42:26 MST 2010
First, I downloaded the 3.3.3 from CodeRed website.
Then I installed it.
I didn't see any install problems.
Then I connected the LPCxpresso board to my laptop USB.
As soon, it was connected, the red link started to blink.
Is this the default?
Then I tried to compile the example and it outputted error related
to missing LPC11xx.h file.
So I searched the c:\nxp subdirectory and found it.
So I then added this in the include search path.
The compiler was able now recognize the include .h file
but now I'm getting the current error without the LPCxpresso board plugged in.

/../arm-none-eabi/bin/ld.exe: cannot find -lCMSISv1p30_LPC11xx
collect2: ld returned 1 exit status
arm-none-eabi-gcc.exe: unrecognized option '-Map=blinky.map'
make: *** [blinky.axf] Error 1

See attachment for screen shot.
Does the LPCxpresso board have to be plugged into the laptop in order for the program to compile properly? Maybe that's my problem.

David
0 Kudos
Reply

2,297 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Mon Apr 12 10:58:55 MST 2010
It builds without any problems for me, using Win7 x64 with V 3.3.3, which I downloaded before it was withdrawn.
0 Kudos
Reply

2,297 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 12 09:48:23 MST 2010
The examples work 'out of the box' so there should be no need to make any changes. Can you explain what you did, step-by-step.
0 Kudos
Reply