BitBanding GPIO Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BitBanding GPIO Voltage

963 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nkarakotas on Tue Jul 24 01:02:28 MST 2012
Hello,

I noticed when using bitbanding on a GPIO the voltage rises up to 2.3V
BITBAND_SRAM_SetBit(LPC_GPIO2_BASE,3);

Why is that?
0 Kudos
Reply
2 Replies

951 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nkarakotas on Tue Jul 24 03:23:27 MST 2012
Hi,

I measured it on an line I have connecting to a LCD, I then removed the lcd and measured the voltage directly. Firstly I didnt use bitbanding and got 3V3. I then used bit banding and toggled the pin and so it rise up to 2.3V.

Regards,
Nick
0 Kudos
Reply

951 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue Jul 24 03:16:43 MST 2012
Hello nkarakotas,

Can you be a bit more specific?

Where did you measure the voltage?
0 Kudos
Reply