Best way to create a custom memory layout?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Best way to create a custom memory layout?

650 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by amrbekhit on Wed Nov 02 15:06:41 MST 2011
Hello all,

I'm porting an existing LPC1752 project from Keil to LPCXpresso 4.1. The is less straightforward than usual because I have a custom memory layout:

///Flash Memory
///StartEndSizeDescription
///0x00000x1FFF0x2000Bootloader
///0x20000xEFFF0xD000Program
///0xF0000xFFFF0x1000Flash Settings
///
///RAM
///StartEndSizeDescription
///0x100000000x10003FDF0x3FE0Application RAM
///0x10003FE00x10003FFF0x0020IAP RAM


It's very easy to implement this memory layout in Keil since the Target dialog box allows you to specify the RO and RW memory ranges directly without having to dive into linker scripts or anything like that. For this project, my ROM starts at 0x2000 and is 0xD000 bytes in size, and my RAM starts at 0x10000000 and is 0x3FE0 bytes in size.

My question is what is the best way to implement this memory layout in LPCXpresso? Reserving the RAM needed for the IAP routines is easy, since there is an FAQ on the subject on the wiki. My main issue is with the ROM layout as I couldn't find any example on the wiki on how to reserve areas of flash. According to the Enhanced Managed Linker Script page on the Wiki, the enhancements are designed to reduce the occurrences where one needs to turn off the feature and take direct control over the linker scripts. Is it possible for me to configure my flash layout without having to manually create my own linker script?

Amr
0 Kudos
Reply
1 Reply

617 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Nov 03 02:30:34 MST 2011
I think that for what you want to do, doing a standard build to create the link scripts, then copying these to another directory and modifying the "mem" script so that the flash starts at a different address would be the best way forward.

For more details, see:

http://support.code-red-tech.com/CodeRedWiki/OwnLinkScripts

Regards,
CodeRedSupport
0 Kudos
Reply