Beginner problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Beginner problems

845件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjallen on Sun May 08 07:12:14 MST 2011
Hi guys,

I'm using an LPC1769 and having major troubles with it. When I first got it LED2 would flash whist it was connected to the USB, I the downloaded the software and went through the beginners guide and tried to download the 'Blinky' example, except I couldn't find that example so I downloaded a different one to it.

That seemed to go fine, except all the board does now is dimly light LED2. I've tried loads of different test programs and it does the same thing, I've also stepped through the different codes which should be changing the status of the LED's and nothing happens.

Like I said, I'm a complete beginner but any advice would be greatley appreciated.

For reference;

Im using Windows Vista,
The original test program was 'rgb'
The ones I've tried since are LPC_flash and LPC_strobe.
0 件の賞賛
返信
2 返答(返信)

836件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjallen on Tue May 10 14:31:23 MST 2011
Works like a charm. Thanks very much!
0 件の賞賛
返信

836件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun May 08 07:28:40 MST 2011
A good start with LPC1769 is 'LPCXpresso1768_systick' sample in  LPCXpresso1768.zip (--> Example folder) :)
0 件の賞賛
返信