Beginner LPCxpresso 1769 + FreeRTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Beginner LPCxpresso 1769 + FreeRTOS

2,220件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glennliu on Mon Jun 03 18:33:43 MST 2013
Hi,

I am a internship student. I am new to both the micro controller and FreeRTOS. I was task to integrate freeRTOS library into the system to achieve task management.

So far, what i did was understanding how freeRTOS work, looking into the details of the hardware of LPC-link 1769 and exploring LPCXpresso software.

Before i proceed, I would like to ask, is it possible to add LAN, WIFI and UART into the system? For LAN there is RD+,RD-,TD+,TD-. For UART, there is UART1/2/3-TX/RX. Can anyone enlighten me, for WIFI. what are the pin needed? Any idea how freeRTOS in general able to help this kind of real time communication

If anyone happen to see any projects that works on this kind of communication, will appreciate that you post the relevant link here to share.  And it will definitely speed up the process of gathering information and will also help future user. I am on internship, and its only 10 weeks, i dont wish to stuck in this project for long. there is more for me to learn :p
0 件の賞賛
返信
7 返答(返信)

1,993件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glennliu on Tue Jun 11 23:12:42 MST 2013
building lpcopen lpc17xx_nxp_xpresso_1769_periph_ethernet project. and face a few problems. how do i know the Ethernet connection is able to transmit and receive ? i already connected the rj45 connector and UART to LPC 1769. but still dont have any data is been send to the UART3.
0 件の賞賛
返信

1,993件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri Jun 07 03:03:51 MST 2013
No, just make sure the missing files are on your include path.
0 件の賞賛
返信

1,993件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glennliu on Fri Jun 07 02:27:41 MST 2013
do i have to manually drag the file into my NXP software include folder?
0 件の賞賛
返信

1,993件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glennliu on Thu Jun 06 18:48:25 MST 2013
hi Code red,

when i build the imported project. it came out errors


C:/Documents and Settings/glennliu/My Documents/LPCXpresso_5.1.2_2065/workspace/New Folder/lpcopen/applications/lpc17xx_40xx/startup_code/cr_startup_lpc17xx40xx.c:48:24: fatal error: sys_config.h: No such file or directory
compilation terminated.
make: *** [cr_startup_lpc17xx40xx.o] Error 1
make: *** Waiting for unfinished jobs....
C:/Documents and Settings/glennliu/My Documents/LPCXpresso_5.1.2_2065/workspace/New Folder/lpcopen/applications/lpc17xx_40xx/examples/periph/periph_ethernet/enet.c:32:19: fatal error: board.h: No such file or directory
compilation terminated.
make: *** [enet.o] Error 1

15:19:07 Build Finished (took 6s.969ms)
0 件の賞賛
返信

1,993件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Jun 06 03:09:46 MST 2013
No. Look at some of the ethernet projects in the examples I previously pointed you at.

Regards,
CodeRedSupport
0 件の賞賛
返信

1,993件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by glennliu on Wed Jun 05 18:29:21 MST 2013
thanks for the reply.

I have to deal with networking communication, Do i have to buy embTCP by freertos/InterNiche? in order to get it working.

embTCP :
http://www.freertos.org/FreeRTOS-Plus/embTCP/FreeRTOS_Plus_TCP.shtml
0 件の賞賛
返信

1,993件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jun 05 01:23:23 MST 2013
Look at the example code bundles supplied in the LPC17 subdirectory of the Examples area of your LPCXpresso installation.

You might also want to take a look at LPCOpen...

http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers

Regards,
CodeRedSupport
0 件の賞賛
返信