Archlinux Installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Archlinux Installation

1,217 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by culyun on Sat Dec 03 02:46:44 MST 2011
Hi,

I'm running an x64 Archlinux installation.
I've created a chroot specifically for i686 applications like LPCXpresso.

The installer runs, but spits the dummy with an exception..

<quote>

failed to allocate font due to internal system font engine problem
    while executing
"$command $path"
    (procedure "Widget::CreateTempWidget" line 11)
    invoked from within
"Widget::CreateTempWidget $tkwidget $tkwidget"
    (procedure "Widget::tkinclude" line 43)
    invoked from within
"Widget::tkinclude Label label .l  remove { -foreground -state -text -textvariable -underline }"
    (in namespace eval "::Label" script line 4)
    invoked from within
"namespace eval Label {
Widget::define Label label DragSite DropSite DynamicHelp

Widget::tkinclude Label label .l  remove { -foreground -state -text -..."
    (procedure "InitGui" line 2546)
    invoked from within
"InitGui"
    (procedure "::InstallJammer::InitializeGui" line 9)
    invoked from within
"::InstallJamgmer::InitializeGui "
    (procedure "::InstallJammer::InitInstall" line 68)
    invoked from within
"::InstallJammer::InitInstall"
    (file "/installkitvfs/main.tcl" line 36106)
</quote>


I see a few people have got LPCXpresso working with Archlinux.
How did you guys do it?

Cheers

Steve
0 Kudos
Reply
1 Reply

1,094 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by culyun on Thu Dec 22 03:36:54 MST 2011
..well the short story is that i got it working.

you need to install ttf-liberation fonts, but i can't remember the other things that i did:(
0 Kudos
Reply