Accessing the SD card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Accessing the SD card

575 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ajay Thallapalli on Wed Apr 08 04:05:09 MST 2015
Hi,

I am using NGX LPC4330 board for my project and I am programming the board by using DFU Programmer.
Could any one have how to access(to see the complete memory., read as well as write) SD card I got two programs

[color=#306]1.lpcopen_2_12_keil_iar_ngx_xplorer_4330\applications\lpc18xx_43xx\keil_uvision_projects\ngx_xplorer_4330\periph\periph_sdmmc[/color]
[color=#393]2.lpcopen_2_12_keil_iar_ngx_xplorer_4330\applications\lpc18xx_43xx\keil_uvision_projects\ngx_xplorer_4330\misc\sdmmc_speed [/color]

1st program i can able to run and work, but 2nd program i can't understand and it is having some problem, while programming it to NGX board using DFU programmer it is showing an error also.

Could any one tell me the solution.
If any one having SD card program (SPIFI mode) please guide me with the program.

Thanking you.
0 项奖励
回复
0 回复数