AFX Load Utility?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFX Load Utility?

951件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by scs on Thu Jan 26 09:37:36 MST 2012
Sorry, I meant AXF Load Utility.

Is there any way to load a <project>.AXF file (or some other objcopy format for an old CodeRed project build) to an LPCXpresso board via USB without using the CodeRed IDE's "Debug" command?  Such as a command line program, CodeRed IDE command, or separate Windows application?
0 件の賞賛
返信
2 返答(返信)

927件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jan 26 09:53:51 MST 2012
Command line?

http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming
0 件の賞賛
返信

927件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Jan 26 09:51:26 MST 2012
There is a flash programming utility built into LPCXpresso. It can be found on the icon bar. It looks like a chip.
0 件の賞賛
返信