ADCR value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADCR value

1,117件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Mon May 24 03:09:10 MST 2010
I use LPC1758 with LPcXpresso.

As per  attached sample, I set a break after the instruction

ADCx-> ADCR =  tmp;

The value to be write in the register ADCR is 0x201100 in hex (look tmp value) , but   the value shown in the register ADCR in the bottom right windows is 3118c (3118c is =  201100 decimal to hexadecimal !!!!!)

In the memory is correct, only the register has the wrong value

Error ??

Thanks
0 件の賞賛
返信
3 返答(返信)

1,103件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon May 24 05:50:45 MST 2010
It is a bug in the display of the value in the peripheral view.
0 件の賞賛
返信

1,103件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Mon May 24 05:34:24 MST 2010

Quote: CodeRedSupport
Thanks for reporting this. It will be fixed in the next release.



Therefore you confirm to me, that is a bug ?
0 件の賞賛
返信

1,103件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon May 24 05:25:08 MST 2010
Thanks for reporting this. It will be fixed in the next release.
0 件の賞賛
返信