ADC sampling at exact time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC sampling at exact time

1,616 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Andrew24 on Thu Apr 29 13:31:41 MST 2010
Hallo. I need ADC to sample two channels every 2ms (500Hz). What is the best way to do this?
0 Kudos
Reply
3 Replies

1,600 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Andrew24 on Fri Apr 30 02:00:26 MST 2010

Quote: leon_heller
Generate an interrupt every 2 ms using a timer.



Thanks for an answer. I did that. where should i switch ADC channels?
0 Kudos
Reply

1,600 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Thu Apr 29 20:25:39 MST 2010
Generate an interrupt every 2 ms using a timer.
0 Kudos
Reply

1,600 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Thu Apr 29 16:48:34 MST 2010
whit a timer, i think so
0 Kudos
Reply