ADC code for the Hitex LPC4300 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC code for the Hitex LPC4300 board

698件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Fri Mar 16 05:54:13 MST 2012
Is there any example code to exercise the four ADC115's on the LPC4300 board, which I am not sure are actually populated?

Thanks,

JohnR[FONT=ArialStandard][SIZE=1][FONT=ArialStandard][SIZE=1]
[/SIZE][/FONT][/SIZE][/FONT]
0 件の賞賛
返信
2 返答(返信)

689件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Sat Mar 17 15:40:14 MST 2012
I have just realised that the current version of this card (-A4) does not contain the 4 ADC1415's, I was looking at the schematic for an earlier version.

Oh well.

JohnR.
0 件の賞賛
返信

689件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Fri Mar 16 05:57:08 MST 2012
I  should have written ADC1415 and also added that I have already searched the LPC knowledge base.

JohnR
0 件の賞賛
返信