A problem on the: LPCXpresso v7 program.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A problem on the: LPCXpresso v7 program.

1,405件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shimon.s on Thu Aug 21 01:06:50 MST 2014
Hi All,

I'm using the: LPCXpresso v7 with the: LPC1343FBD48 chip.
I'm getting the attached problem (When I'm trying to download the program to the External device) and I've:
Closed the program.
Restarted the PC.
But the problem continues, I'll be happy for any idea to solve the problem

On the Console I'm getting the following info: The target endianness is set automatically (currently little endian)
/home/build/work/GCC-4-8-build/src/gdb/gdb/linespec.c:2445: internal-error: decode_line_full: Assertion `state->canonical_names.suffix != NULL' failed.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Quit this debugging session? (y or n) [answered Y; input not from terminal]
/home/build/work/GCC-4-8-build/src/gdb/gdb/linespec.c:2445: internal-error: decode_line_full: Assertion `state->canonical_names.suffix != NULL' failed.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Create a core file of GDB? (y or n) [answered Y; input not from terminal]

This application has requested the Runtime to terminate it in an unusual way.
Please contact the application's support team for more information.


Thanks,
Shimon.
0 件の賞賛
返信
3 返答(返信)

1,375件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shimon.s on Sat Aug 23 22:53:56 MST 2014
Hi,

10X a lot for your mail reply.
Regarding your question I'm using the: LPCXpresso v7.3.0 [Build 186] [2014-07-09]

10X,
Shimon.
0 件の賞賛
返信

1,375件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Aug 21 04:02:17 MST 2014
I am glad that you found a solution.

It would be helpful if you could provide a means of replicating the problem here though so that we can investigate further. A buildable project with instructions on how to trigger the fault would be ideal!

http://www.lpcware.com/content/faq/lpcxpresso/how-importexport-projects

Please also confirm which version of LPCXpresso you are actually using - 7.3.0 ??

Regards,
LPCXpresso Support
0 件の賞賛
返信

1,375件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shimon.s on Thu Aug 21 02:40:13 MST 2014
Hi All,

The problem solution was to remove the disabled breakpoints.

10X,
Shimon.
0 件の賞賛
返信