1769 pwm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1769 pwm

891件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1769user on Wed Jan 30 02:31:16 MST 2013
I am having problems getting this to generate a couple of PWM outputs. Has anyone a comprehensive list of the registers that need to be initialised? Better still would be a commented example.
Many thanks.
0 件の賞賛
返信
2 返答(返信)

846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1769user on Wed Jan 30 07:34:21 MST 2013
I tried searching but couldn't find anything useful.
For example, there is a problem with PWMLER. It seems that this is only reset to zero by a match if bit 0( for MR0) is set? If I set the bits for MR5 and MR6, these remain set. If I set bit 0, all the bits are reset.
Trial and error is a very slow process.
0 件の賞賛
返信

846件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jan 30 02:56:17 MST 2013

Quote: 1769user
Better still would be a commented example.



:confused:

There are several threads about LPC1769 PWM like:

http://knowledgebase.nxp.com/showthread.php?p=16360

A simple search could help :)
0 件の賞賛
返信