1343 USB Question.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1343 USB Question.

893件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ub3r on Tue Jul 03 02:01:07 MST 2012
Hi Guys

Whats the easiest way to set/read some variables on the LPC1343 via USB??

Also, is the source code for the 'LPC1343 HID Demonstration' windows app available? I've managed to get this working, but i would like to see the source code for windows application so i can make my own.

cheers
0 件の賞賛
返信
1 返信

877件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jul 03 03:42:18 MST 2012

Quote: ub3r
Hi Guys

Whats the easiest way to set/read some variables on the LPC1343 via USB??




Hi Guy, that's CDC ;)
0 件の賞賛
返信