How to import/export projects

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to import/export projects

7,664件の閲覧回数
lpcware-support
Senior Contributor I

Import/Export projects

Import and Export should be used to move projects between workspaces or computers. This will ensure project settings are correctly transferred.

Exporting projects

We recommend that before exporting a project, you perform a "Clean" build to remove binary executable and object files from the build. These are not normally required, and this will make the exported archive significantly smaller.

To export a project:

  • Select the project (or projects) in the Project explorer
    • Use Ctrl-Click to select more than one project
  • In the Quickstart Panel, click on:
    • Click on Export project to archive (zip) or
    • Export project and references to archive (zip)
  • Enter or Browse the zip file name and then Finish

Your project is now exported

Importing projects

To import an archive containing one or more projects into the workspace, including the Examples provided with the LPCXpresso IDE:

  • To Import projects.
  • In the Quickstart Panel, click on Import projects
  • If Importing from a zip file, press the Archive Browse button
    • Browse to the zip file, and press OK
  • If you are importing projects from a directory, press the Root directory Browse button
    • Browse to the directory containing the projects, and press OK
  • A list of importable projects contained in the directory is displayed
  • Check/uncheck projects from the list as necessary and Finish

The projects will now be imported.

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)