Gray folders

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gray folders

Jump to solution
6,157 Views
mariob
Contributor III

Hi,

I try to implement a Vcom Port (CDC) on an PN7462. I need to use USBD_ROMStack.

But this folder is greyed out and strike through. I searched a lot, but wasn't able to find the meanig

of the grey folders and files.

Gray folders.jpg

Im sure this is no big issue.

Best Regards 

Mario

Labels (1)
0 Kudos
Reply
1 Solution
4 Replies
5,585 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Are these folder perhaps marked as excluded from the build? Right click on them in the Project Explorer view and check the settings in the "Resouce Configurations" entry.

I also note that your project is using linked references. Make sure these folders actually exist in the linked location.

Regards,

LPCXpresso Support

0 Kudos
Reply
5,585 Views
mariob
Contributor III

Hi,

thank you for your reply. No this files are not excluded from the build. The folders are 

also existing. It's from the PN7462 examples witch you can download from here:

PN746X_736X_SERIES|NXP 

Best Regards

Mario

0 Kudos
Reply
5,585 Views
mariob
Contributor III

Hi Con Verse,

thank you very much. This solved my problem.

Best Regards 

Mario

0 Kudos
Reply