All SWD targets are currently connected to other debug sessions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

All SWD targets are currently connected to other debug sessions

4,945件の閲覧回数
lpcware-support
Senior Contributor I

In LPCXpresso IDE if you attempt to start a debug session whilst there is already an existing debug session made, then you will see the error of the form:

All SWD targets are currently connected to other debug sessions

You will need to terminate the existing debug session before starting a new one. To do this, switch to the Debug View and select the current application being debugged. You should then be able use the "Terminate" or "Terminate All" buttons on the icon bar.

Once this is done, select the project you now want to debug in the Project Explorer view, then use the Debug entry on the Quickstart view to start your new debug session.

Note that if you see this error and there is no currently active debug session, then try terminating the 'redlinkserv' process directly. To do this, switch to the "RedlinkServer" Console, and click on the "Kill server" button.

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)