why the spinbox disable receive the input focus when use TAB key?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why the spinbox disable receive the input focus when use TAB key?

1,175 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ling3wei on Mon Nov 19 21:36:29 MST 2012
why the spinbox disable receive the input focus when use TAB key?
I will be using a Spinbox widget without a touch or mouse interface, only using the,tab, up, down, left, right,enter,space keys of a keyboard. the other widget is able to receive the input foucs but the spinbox can`t.
My code :
static const GUI_WIDGET_CREATE_INFO _aDialogCreate[] = {
  { FRAMEWIN_CreateIndirect, "", ID_FRAMEWIN_0, 0, 35, 331, 328, 0, 0, 0 },
  { BUTTON_CreateIndirect, "", ID_BUTTON_0, 68, 225, 85, 50, 0, 0, 0 },
  { BUTTON_CreateIndirect, "", ID_BUTTON_1, 202, 225, 85, 50, 0, 0, 0 },
  { SPINBOX_CreateIndirect, "", GUI_ID_SPINBOX0_11, 2, 2, 65, 40, 0, 0, 0 },
};
Labels (1)
0 Kudos
Reply
0 Replies