using SGPIO on LPC4370 in LPC-link2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using SGPIO on LPC4370 in LPC-link2

1,698件の閲覧回数
robotxyz
Contributor I

Hi,

  I am having basic trouble in locating/using the SGPIO pin in LPC-link2 board. To make things simple, I am trying to setup the SGPIO pin as a GPIO pin. Please take a look at the code lines below. The code is getting into the runpincheck2() and seems to loop through fine because the board led is toggling as expected. However I do not see the SGPIO13 set as a GPIO pin toggling.

  In the LPC-link2 board SGPIO13 pin is buffered from P2_4 and is connected to jumper connector J4_pin18. When I monitor J4_pin18 the pin is not toggling (pin seems to be floating as it is varying randomly near ground; does not seem to be strongly connected to ground).

#if defined (__USE_LPCOPEN)
    // Read clock settings and update SystemCoreClock variable
    SystemCoreClockUpdate();
#if !defined(NO_BOARD_LIB)
#if defined (__MULTICORE_MASTER) || defined (__MULTICORE_NONE)
    // Set up and initialize all required blocks and
    // functions related to the board hardware
    Board_Init();
#endif
    // Set the LED to the state of "On"
    Board_LED_Set(0, true);
#endif
#endif

runpincheck2();

void runpincheck2(void){
    Chip_SCU_PinMuxSet((uint8_t)0x2, (uint8_t)4, (uint16_t)(SCU_MODE_INACT | SCU_MODE_FUNC0) );
    LPC_SGPIO->OUT_MUX_CFG[13] = (0L << 4) | (4L << 0);
    LPC_SGPIO->GPIO_OENREG |= (1L <<13);
    while(1){
        volatile int i, junki;
        LPC_SGPIO->GPIO_OUTREG |= (1L << 13);
        Board_LED_Toggle(0 );
        for(i=0; i<1000000; i++) {
            junki++;
        }
        LPC_SGPIO->GPIO_OUTREG &= ~(1L << 13);
        Board_LED_Toggle(0 );
        for(i=0; i<4000000; i++){
            junki++;
        }
    }
    return;
}

Thanks,

robotxyz

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,540件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello robot xyz,

I have reply you on your salesforce case, please check.

BR

Alice

0 件の賞賛
返信