serial problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

serial problem

2,397 Views
aravindpb5009
Contributor III

hai

when i try to enter some value in serial port that time my entered value doesn't print in the serial as well as o/p also not coming   please let me know the solution

In below i attached my error snaps please find the attachments below   

Thanks & Regards 

Aravind P

Labels (1)
0 Kudos
Reply
2 Replies

2,337 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aravind P,

In this board, the Micro USB port(J3) only can send character, can't receive, because only the UART_TX connect to it.

So when run this demo, please connect the UART to your PC using TTL to USB.

In this demo,  USART0_TXD connect to P0_7     USART0_RXD connect to P0_18 .

I test on my side ,it can work well:

pastedImage_1.png

pastedImage_3.jpg

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,337 Views
aravindpb5009
Contributor III

Thank you for your valuable assistance  

0 Kudos
Reply