rehost lpc2378

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

rehost lpc2378

1,503件の閲覧回数
mikemillsap
Contributor I

We have legacy code written for LPC2378 that we need to rehost on an LPC4088 (new part on redesigned board).

Just thought I would start here and ask if anybody has opinions on the best approach to begin with?
Has anybody out there gone through this recently?
What are the things/"low hanging fruit" that I should be concerned about first?

I am using IAR EWARM IDE.

Thanks!

ラベル(3)
0 件の賞賛
返信
1 返信

1,317件の閲覧回数
b36401
NXP Employee
NXP Employee

Please note that LPC2378 and LPC4088 processors have different memory map, different interfaces and even different ARM cores.
So you need to review all code in point of processor specific.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信