problem with nxp lpc 11u24/301: can't open virtual com after running cdc usb rom driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with nxp lpc 11u24/301: can't open virtual com after running cdc usb rom driver

890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marcello.ioppolo on Fri Sep 13 01:53:13 MST 2013
hello everybody,

i run the cdc usb virtual com examples found at:

http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso

on my lpc11u24/301 microcontroller but after connecting the usb cable and visualizing correctly the virtual com i can't open the port with a serial data logger or any other software.

i imported the entire folder containing the cdc usb rom example and the build happens to be correct so it is the debugging.

what's wrong with my virtual com? i use windows xp and the driver provided by nxp support for letting the virtual com appears.

thank you very much for helping with this.

best regards
Labels (1)
0 Kudos
Reply
2 Replies

866 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Tue Jan 27 09:50:00 MST 2015
Hi Marcello,
You may have issue similar to below thread.
http://www.lpcware.com/content/forum/lpc11u14-api-software-could-not-detect-com-port-after-re-plug-h...
0 Kudos
Reply

866 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wilson.lee on Mon Jan 26 07:16:36 MST 2015
same issue with you
0 Kudos
Reply