phasing out LPC2000 series?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

phasing out LPC2000 series?

3,042 Views
jeffreycasey
Contributor I

I see that most of the LPC2xxx line is now marked "not recommended for new designs".    Are these being phased out?   What is the expected timeline?

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

2,883 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jeffrey Casey

Normally LPC2xxx has 15 years longevity time. This means we can ensure a stable supply for this product for 15 years from the product launch time.

Which LPC2xxx chip do you work with specifically? I can check and confirm.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,883 Views
jeffreycasey
Contributor I

Thanks!

I use many in the series in a number of active client designs....and

many are on "no changes" production contracts

for several years in the semi- industry.    This is a serious concern.

I particularly use the LPC2103FBD48 and LPC2131 or LPC2138  for some

commercial clients with ongoing production.

I also particularly use the LPC2377FBD144,  the LPC2387FBD100,  the

LPC2388FBD144,  and the LPC2468FBD208 for

custom jobs.   In particular, I'm quoting out a new military radar job

right now using a couple of the latter bunch, and am very concerned.

Thanks!

Jeff Casey

Rockfield Research Inc.

Las Vegas, NV, USA

0 Kudos
Reply

2,883 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jeff,

Please FYI

LPC2103FBD48: launch data Feb 2008, 15years

LPC2131FBD64: Launch date May 2006, 15years

LPC2138FBD64: launch date Dec 2008, 15 years

LPC2138FHN64: launch date Aug 2006, 15years.

LPC2377FBD144: launch data Feb 2008, 15years

LPC2387FBD100: Launch date Nov 2007, 15years

LPC2388FBD144: launch data Feb 2008, 15years

LPC2468FBD208: launch data Feb 2008, 15years


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply