need help with Can module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

need help with Can module

1,235 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mary Cilna on Wed Nov 12 23:46:26 MST 2014
hi,
i have configured my Can 2.  i dont have enough knowledge to configure the bus timing registers.
i want to communicate with bus bit rate of 1 Mbps. what should be my baud rate ? the can module works with a clock of 60 MHz. Is it possible to establish  the communication with this clock frequency ?

when the Can_Send_msg() function is called the Transmission Complete Status bit is set to '0' and am not able to receive any data in the receiving end . it happened to repeat with all the transmit buffers. why is it so ? i am new to CAN also .

Labels (1)
0 Kudos
Reply
1 Reply

1,201 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Tue Dec 02 14:15:56 MST 2014
Hi, Mary,
Have you tried to run the sample project periph_can? and use it as a reference to setup your software?
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc40xx-packages

Thanks,
0 Kudos
Reply