lpx43xx usb0 host HID keyboard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpx43xx usb0 host HID keyboard

2,813件の閲覧回数
shivrajtbm
Contributor I

HI 

i'm using lpx4357 and successfully completed keyboard interfacing using USB HID but when i connect a barcode scanner hard fault occurs after scanning .. only one byte read / detected and then it goes to hard fault.. can i get some ideas why this could be happen?? or any suggestions ?

 

please help!

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,805件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Is your project based on lpcopen demo ? if yes which one? any revise ?

Please track where runs to error? Does it enumerate well?

0 件の賞賛
返信

2,789件の閲覧回数
shivrajtbm
Contributor I

issue solved .. thank you..

0 件の賞賛
返信

2,110件の閲覧回数
Md_Rdgc
Contributor I

Hi,

I am trying to interface the USB barcode scanner. I am using the LPCOpen Keyboard Host example, I am getting the keyboard keys. But when I connect the barcode scanner, it shows device is enumerated, but now able to read the barcode data. Can you please let me know, what modification need to be done in the keyboard code example to read the barcode data. 

Controller LPC4337

Barcode Make Newland.

Model NLS-HR11

Warm regards.

 

0 件の賞賛
返信