lpc54018 credit based shaper

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc54018 credit based shaper

6,382 Views
wwang
Contributor I

Does LPC54018 support credit based shaper, if yes, how can I enable it ?

0 Kudos
Reply
13 Replies

6,358 Views
magicoe_niu
NXP Employee
NXP Employee

@william_jiang would you mind assign a guy support this case who knows Ethernet IP well? 

The end customer is Microsoft

 

Thank you!
0 Kudos
Reply

6,265 Views
wwang
Contributor I

Hi Magicoe,

any update on this topic?

is there any special requirement for enabling CBS? 

we run traditional iperf test on queue enabled CBS, and expect the throughput are limited by the idle slope. Is that reasonable?

 

0 Kudos
Reply

6,370 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I do not think that the Ethernet module of LPC54018 supports credit based shaper.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

6,225 Views
wwang
Contributor I

Hi,

have you received the project I send out by e-mail?

thanks.

0 Kudos
Reply

6,222 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

Can you clarify your requirement? do you hope that NXP engineer can help review your code, or you do not know how to use CBS feature of ethernet and hope to get support.

Pls clarify your requirements.

BR

XiangJun Rong

 

 

0 Kudos
Reply

6,212 Views
wwang
Contributor I

1. if LPC54018 support CBS?

2. if yes, how to enable it.

if the question 2 is too complicate, let us ignore it.

I think just to clarify if LPC54018 supports CBS, that will be good enough.

0 Kudos
Reply

6,201 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

This is the AE reply "LPC54018 supports CBS", but we have not the code to support the feature in SDK driver. I am sorry.

BR

XiangJun Rong

 

0 Kudos
Reply

6,349 Views
wwang
Contributor I

Thanks for the information.

I just created the code based on the reference manual :  UM11060
LPC540xx/LPC54S0xx User manual.

and there are actually credit based shaper register on LPC54018

 

0 Kudos
Reply

6,338 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Obviously, from the UM11060.pdf, the LPC54018 supports CBS, I will create a ticket for AE team, pls clarify your requirements so that the AE team engineer can help you

If you require  us to review the code, pls post it here or send to my personal Email if it is confidential.

BR

XiangJun Rong

0 Kudos
Reply

6,335 Views
wwang
Contributor I

ok, i can send you the CBS code to review, can you tell me your email?

Do you have examples that show how to use CBS and how to validate the CBS function?

0 Kudos
Reply

6,286 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I tried to contact you, but it appears that your Email address has issue. Pls check if the spelling is correct.

[email protected]

BR

Xiangjun Rong

0 Kudos
Reply

6,278 Views
wwang
Contributor I

thanks for the effort, that email can't be accessed.

i will leave my personal email here: [email protected]

0 Kudos
Reply

6,346 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

I appologize for the wrong information, I am not familiar with the CBS (credit based shaper) protocol.

We will give you a response after we discuss with AE team engineers.

BR

XiangJun Rong

0 Kudos
Reply