lpc54018 credit based shaper

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc54018 credit based shaper

6,380件の閲覧回数
wwang
Contributor I

Does LPC54018 support credit based shaper, if yes, how can I enable it ?

0 件の賞賛
返信
13 返答(返信)

6,356件の閲覧回数
magicoe_niu
NXP Employee
NXP Employee

@william_jiang would you mind assign a guy support this case who knows Ethernet IP well? 

The end customer is Microsoft

 

Thank you!
0 件の賞賛
返信

6,263件の閲覧回数
wwang
Contributor I

Hi Magicoe,

any update on this topic?

is there any special requirement for enabling CBS? 

we run traditional iperf test on queue enabled CBS, and expect the throughput are limited by the idle slope. Is that reasonable?

 

0 件の賞賛
返信

6,368件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I do not think that the Ethernet module of LPC54018 supports credit based shaper.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

6,223件の閲覧回数
wwang
Contributor I

Hi,

have you received the project I send out by e-mail?

thanks.

0 件の賞賛
返信

6,220件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

Can you clarify your requirement? do you hope that NXP engineer can help review your code, or you do not know how to use CBS feature of ethernet and hope to get support.

Pls clarify your requirements.

BR

XiangJun Rong

 

 

0 件の賞賛
返信

6,210件の閲覧回数
wwang
Contributor I

1. if LPC54018 support CBS?

2. if yes, how to enable it.

if the question 2 is too complicate, let us ignore it.

I think just to clarify if LPC54018 supports CBS, that will be good enough.

0 件の賞賛
返信

6,199件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

This is the AE reply "LPC54018 supports CBS", but we have not the code to support the feature in SDK driver. I am sorry.

BR

XiangJun Rong

 

0 件の賞賛
返信

6,347件の閲覧回数
wwang
Contributor I

Thanks for the information.

I just created the code based on the reference manual :  UM11060
LPC540xx/LPC54S0xx User manual.

and there are actually credit based shaper register on LPC54018

 

0 件の賞賛
返信

6,336件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Obviously, from the UM11060.pdf, the LPC54018 supports CBS, I will create a ticket for AE team, pls clarify your requirements so that the AE team engineer can help you

If you require  us to review the code, pls post it here or send to my personal Email if it is confidential.

BR

XiangJun Rong

0 件の賞賛
返信

6,333件の閲覧回数
wwang
Contributor I

ok, i can send you the CBS code to review, can you tell me your email?

Do you have examples that show how to use CBS and how to validate the CBS function?

0 件の賞賛
返信

6,284件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I tried to contact you, but it appears that your Email address has issue. Pls check if the spelling is correct.

[email protected]

BR

Xiangjun Rong

0 件の賞賛
返信

6,276件の閲覧回数
wwang
Contributor I

thanks for the effort, that email can't be accessed.

i will leave my personal email here: [email protected]

0 件の賞賛
返信

6,344件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

I appologize for the wrong information, I am not familiar with the CBS (credit based shaper) protocol.

We will give you a response after we discuss with AE team engineers.

BR

XiangJun Rong

0 件の賞賛
返信