lpc43xx_DualCore_Eamples_V0.1 DO NOT COMPILE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc43xx_DualCore_Eamples_V0.1 DO NOT COMPILE

1,144件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marshall on Thu Oct 25 09:41:05 MST 2012
There is at least 1 missing file lpc_emac_config.h, does anyone know where to get this?
ラベル(1)
0 件の賞賛
返信
1 返信

1,128件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by marshall on Thu Oct 25 10:47:56 MST 2012
More information the entire lwip directory is missing, and lwipopts.h When I unzip the lwip_lpc.zip it is of course not in the correct directory naming that was expected. I am browsing the internet and having to cut and paste include files where I expect them to go, is this the desired approach?

Is there a zip file that will add the lwip, and any other missing directories needed to compile these dual core examples?
0 件の賞賛
返信