lpc11xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc11xx

866件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Fri May 20 09:43:50 MST 2011
<h2 class="indent">Introduction</h2>
<div class="indent"><span class="inline inline-left"><img class="image image-preview " src="http://www.lpcware.com/system/files/images/LPC1100XL%20block%20diagram_crop.preview.jpg" border="0" alt="" title="" width="565" height="640" /></span></div>
<div class="indent">The ARM<sup>®</sup> Cortex™-M0 processor is the smallest, lowest-power and most energy-efficient ARM processor available. The exceptionally small silicon area, low power, and minimal code footprint of the processor achieves 32-bit performance at an 8-bit price point, bypassing the step to 16-bit devices.</div>
<div class="indent">The Cortex-M0 processor promises substantial savings in system cost while retaining tool and binary compatibility with feature-rich processors such as the Cortex-M3 processor. It consumes as little as 85 microwatts/MHz (0.085 milliwatts) in an area of typically under 12K gates, enabling the creation of ultra low-power analog and mixed signal devices.</div>
ラベル(1)
0 件の賞賛
返信
0 返答(返信)