load only u-boot and not kernel on lpc3250 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

load only u-boot and not kernel on lpc3250 board

925件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kamini on Wed May 08 04:58:08 MST 2013

Hi,


<p style="text-align: justify;">I am using a mini3250 from embest. I want to load only u-boot onto the mini3250 and not the kernel. In user manual i
could not find how to get u-boot prompt on hyperterminal. I also want to make some  changes to the source code of u-boot. which folder inside Mini3250_100304/Source/Bootloader/u-boot-1.3.3/board would contain the code of mini 3250?
Any suggestion or pointers will be helpful.

Thanks,
Kamini
ラベル(1)
0 件の賞賛
返信
0 返答(返信)