if is the LPC1765`s SPI not support so high frequece when as slave?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

if is the LPC1765`s SPI not support so high frequece when as slave?

565件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by carson84 on Wed Mar 30 23:23:23 MST 2016
spi port:
p[0].15, --> SCK
p[0].16, --> SSEL
p[0].17, --> MISO
p[0].18, --> MOSI

I use LPC1765`s SPI (slave mode) to communicate with another device.(MTK3360, spi, master mode)
when the clock frequece up to 1Mkz, the LPC1765`s SPI send wrong data out. (below 500KHZ, it is normal)

if is the LPC1765`s SPI not support so high frequece when as slave?
ラベル(1)
0 件の賞賛
返信
1 返信

549件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信