hwCAN_MsgTransmit fail with bit0error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hwCAN_MsgTransmit fail with bit0error

1,387 Views
thomasjohansen
Contributor I


Hi,

 

Im using the sample "ccan_rom" from the lpcopn 2.20 with my own hardware platform.

The CAN high and low are located on pin 13 and 18. TJA1051 used.

 

But when I call the hwCAN_MsgTransmit i get an Bit0Error? I can't even moved the TD/RD pins in test mode?

The TJA1051 is connected correct..

 

Any idea's?

 

Thomas

Tags (1)
0 Kudos
Reply
1 Reply

1,235 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Thomas,

Could you tell us which LPC MCU are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply