how to interface at24c256 I2C eeprom to lpc2148? can any one help me ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to interface at24c256 I2C eeprom to lpc2148? can any one help me ?

3,546 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by j.hariharan30 on Thu Dec 10 01:02:59 MST 2015
can any one guide me to do the procedure for eeprom interface with lpc2148. I will tried with that interface but it not done properly,so plz anyone help me to do this task.
Labels (1)
0 Kudos
Reply
3 Replies

3,054 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mazaumesh on Mon May 02 22:47:18 MST 2016
Dear Hariharan,

I have spent enough time to test 24LC512 EEPROM with LPC2148. I have written post and shared complete source code and circuit diagram. If I write all little details again here then I will run out of time. Here is link: http://www.binaryupdates.com/i2c-in-lpc2148-arm7-microcontroller/

If in case you have any question then feel free to write me.

Good Luck !!!
0 Kudos
Reply

3,051 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by j.hariharan30 on Thu Dec 10 22:54:43 MST 2015
Thank you for your reply sir,
                                  I already have that code bundle but in those I2C folder abstract shows, it has interface with PCF8594C-2 EEPROM. I want to interface with at24c256 EEPROM, so i want to know it is possible or not. I have to run I2C program in keil and debug with I2C0 interface, when the program run it has not displayed proper protocol status, it only displayed device address and negative ACK only. I have to tried with proteus software to simulate, it  also displayed and hold start condition only.
Here as i attached response window of keil and proteus.
0 Kudos
Reply

3,051 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Dec 10 06:55:59 MST 2015
Hi,
Could you please describe the problem you are facing. You can use I2C example from code bundle which is at below location
https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc213xlpc214x-peripherals-using-keils-%C...
0 Kudos
Reply