how to calculate EMAC variables located in 16K Ethernet SRAM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to calculate EMAC variables located in 16K Ethernet SRAM?

647 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sadegh.rabei on Mon Mar 14 11:34:42 MST 2016
Hello there,

i got a question about the easyweb example for the lpc1768.

Here's how to calculate the highlighted lines?

thank you.


[color=#c00]#define NUM_RX_FRAG         4           /* Num.of RX Fragments 4*1536= 6.0kB */
#define NUM_TX_FRAG         3           /* Num.of TX Fragments 3*1536= 4.6kB */ [/color]
#define ETH_FRAG_SIZE       1536        /* Packet Fragment size 1536 Bytes   */

#define ETH_MAX_FLEN        1536        /* Max. Ethernet Frame Size          */

/* EMAC variables located in 16K Ethernet SRAM _ bank 1 */
#define RX_DESC_BASE        0x20080000
#define RX_STAT_BASE        (RX_DESC_BASE + [color=#c00]NUM_RX_FRAG*8[/color]) // 4*(2*4)
#define TX_DESC_BASE        (RX_STAT_BASE + [color=#c00]NUM_RX_FRAG*8[/color]) // 4*(2*4)
#define TX_STAT_BASE        (TX_DESC_BASE + [color=#c00]NUM_TX_FRAG*8[/color]) // (4-1)*(2*4)
#define RX_BUF_BASE         (TX_STAT_BASE +[color=#c00] NUM_TX_FRAG*4[/color]) // (4-1)*(1*4)
#define TX_BUF_BASE         (RX_BUF_BASE  + [color=#c00]NUM_RX_FRAG*ETH_FRAG_SIZE[/color])

/* RX and TX descriptor and status definitions. */
#define RX_DESC_PACKET(i)   (*(unsigned int *)(RX_DESC_BASE   + 8*i))
#define RX_DESC_CTRL(i)     (*(unsigned int *)(RX_DESC_BASE+4 + 8*i))
#define RX_STAT_INFO(i)     (*(unsigned int *)(RX_STAT_BASE   + 8*i))
#define RX_STAT_HASHCRC(i)  (*(unsigned int *)(RX_STAT_BASE+4 + 8*i))
#define TX_DESC_PACKET(i)   (*(unsigned int *)(TX_DESC_BASE   + 8*i))
#define TX_DESC_CTRL(i)     (*(unsigned int *)(TX_DESC_BASE+4 + 8*i))
#define TX_STAT_INFO(i)     (*(unsigned int *)([color=#c00]TX_STAT_BASE   + 4*i[/color]))
#define RX_BUF(i)           ([color=#c00]RX_BUF_BASE + ETH_FRAG_SIZE*i[/color])
#define TX_BUF(i)           ([color=#c00]TX_BUF_BASE + ETH_FRAG_SIZE*i[/color])
标签 (1)
0 项奖励
回复
1 回复

622 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复