how is vcom_bread supposed to work?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how is vcom_bread supposed to work?

1,383 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sjondur on Mon Nov 02 15:08:22 MST 2015
What happens when you read the com buffer in multiple segments?

In its current form it will copy from the same location again and again when the function is called repeatedly:
memcpy(pBuf, pVcom->rx_buff, cnt);

why not do
memcpy(pBuf, pVcom->rx_buff + rx_rd_count, cnt);  
etc...

cdc_vcom.c
/* Virtual com port buffered read routine */
uint32_t vcom_bread(uint8_t *pBuf, uint32_t buf_len)
{
VCOM_DATA_T *pVcom = &g_vCOM;
uint16_t cnt = 0;
/* read from the default buffer if any data present */
if (pVcom->rx_count) {
cnt = (pVcom->rx_count < buf_len) ? pVcom->rx_count : buf_len;
memcpy(pBuf, pVcom->rx_buff, cnt);
pVcom->rx_rd_count += cnt;

/* enter critical section */
NVIC_DisableIRQ(USB0_IRQn);
if (pVcom->rx_rd_count >= pVcom->rx_count) {
pVcom->rx_flags &= ~VCOM_RX_BUF_FULL;
pVcom->rx_rd_count = pVcom->rx_count = 0;
}
/* exit critical section */
NVIC_EnableIRQ(USB0_IRQn);
}
return cnt;

}
Labels (1)
0 Kudos
Reply
0 Replies