hitex_eva_4350_usbd_rom_cdc_vcom Example - Failed to open the virtuell Com port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hitex_eva_4350_usbd_rom_cdc_vcom Example - Failed to open the virtuell Com port

1,438 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Meyer on Fri Nov 22 06:03:43 MST 2013
Hi Lpc-Team,

I downloaded the new Lpcopen Examples V2.02 and compile  the above-mentioned Example. All Fine no Errors. I downloaded the Windows drivers (lpcopen_examples_windows_usb_drivers_v1_10.zip) and installed the Driver. The device is recognized as a virtual comport (Com6). As a reminder, I use the hitex board 4350.

Now I wanted to test the "echo" and open my hyperterminal Putty. Putty reports an error when opening the Comport. Ok I switch to Hterm and here error when opening, too.

Is there someone who has ready a solution ? an Idea? who fix the problem ?


I am grateful for any help ;)

Thx
Best regards

Meyer Thomas

Labels (1)
0 Kudos
Reply
1 Reply

1,423 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by durgesh on Wed Dec 04 18:33:36 MST 2013
You could use Teraterm or implement the workaround discussed in this thread.


0 Kudos
Reply