hitex_eva_4350_usbd_rom_cdc_vcom Example - Failed to open the virtuell Com port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hitex_eva_4350_usbd_rom_cdc_vcom Example - Failed to open the virtuell Com port

1,446件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Meyer on Fri Nov 22 06:03:43 MST 2013
Hi Lpc-Team,

I downloaded the new Lpcopen Examples V2.02 and compile  the above-mentioned Example. All Fine no Errors. I downloaded the Windows drivers (lpcopen_examples_windows_usb_drivers_v1_10.zip) and installed the Driver. The device is recognized as a virtual comport (Com6). As a reminder, I use the hitex board 4350.

Now I wanted to test the "echo" and open my hyperterminal Putty. Putty reports an error when opening the Comport. Ok I switch to Hterm and here error when opening, too.

Is there someone who has ready a solution ? an Idea? who fix the problem ?


I am grateful for any help ;)

Thx
Best regards

Meyer Thomas

ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,431件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by durgesh on Wed Dec 04 18:33:36 MST 2013
You could use Teraterm or implement the workaround discussed in this thread.


0 件の賞賛
返信