flash driver failed to initialize

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flash driver failed to initialize

1,337 Views
Sathiya_T
Contributor I

When flash with support on ULINK2 debugger the GPIO example code in LPC804 , Flash deriver failed to initialize error is occured continuosly.

0 Kudos
Reply
1 Reply

1,283 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that you use NXP manufactured LPCXpresso804 boards, if it is the case, you have to disable on board debugger by closing the JP1 and connect the SWD signal to CN1 of LPCXpresso804 boards.

 

xiangjun_rong_0-1686533288576.png

SWD connector CN1 signals assignment

xiangjun_rong_1-1686533442940.png

On the IDE, you can delete the *debug.lauch file so that the tools can research the device.

If you use your own board, I am sorry.

Hope it can help you

BR

Xiangjun Rong

 

0 Kudos
Reply