failed DDR DQS Auto calibration-LPC3250

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

failed DDR DQS Auto calibration-LPC3250

1,671件の閲覧回数
justinvil1103
Contributor I

Hi,

 

We are running a DDR test and the following feature of the LPC3250 "DDR DQS Auto calibration" kept failing. We do not know what cause it to fail, any help would be greatly appreciated.

 

Thanks,

WJ

0 件の賞賛
返信
2 返答(返信)

1,650件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Normally the DDR problems are due to hardware issues,

Do all the lines have the same impedance?

there are some application notes with recommendations about DDRs 

https://www.nxp.com/docs/en/application-note/AN10935.pdf

I hope this will help you.

 

0 件の賞賛
返信

1,637件の閲覧回数
justinvil1103
Contributor I

 

Hi Vicente,

We have a one-time calibration at boot up, what would happen if we turn the "Auto Calibration" off? or disable it?                                                                                                                                         
 
 
 
 
 
 
 
 
Thanks,                                                                                                                                                             WJ
 
 
 
 
 
 
 
0 件の賞賛
返信