emwin deployment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emwin deployment

2,291 Views
nithin3200
Contributor IV

Hi

 

Am using Emwin for LPC546xxx with customized board.Display model number is TM104SDHG05, Tianma model. Anyone can suggest me how i can initialize  emwin.                                                                                                                                  

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

2,280 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

There is emwin_examples under SDK, you can refer to:

Alice_Yang_0-1658718644171.png

 

BR

Alice

 

0 Kudos
Reply

2,269 Views
nithin3200
Contributor IV

 

@xiangjun_rong 

 

Thanks for your reply and  we have downloaded the  emwin sdk for lpc546xx and integrated the emwin libraries in our project  currently we are facing the issue of  in the GUI_init();So  far we have  not used the debugger in our project and we are using the uart for verifying the program flow .

as per program flow:

GUI_INIT----------------->LCD_INIT-------------->Hung or may be in hardfault exceptions.

 

We are using the external ram for storing the display buffer and gui buffer .Please go through the images i have attached for your reference.

We ae using tianma lcd part number TM104SDHG05

--------------------CODE-------------------------------------

#include "FreeRTOS.h"

#include "task.h"

#include "queue.h"

#include "timers.h"

#include "semphr.h"

#include "GUI.h"

#include "WM.h"

#include "GUIDRV_Lin.h"

#include "board.h"

#include "fsl_ctimer.h"

#include "fsl_sctimer.h"

#include "fsl_gpio.h"

#include "fsl_lcdc.h"

#include "fsl_i2c.h"

#include "fsl_usart.h"

#include <cr_section_macros.h>

 

 

#include "fsl_device_registers.h"

#include "pin_mux.h"

#include "board.h"

#include "stdint.h"

 

#include "DIALOG.h"

 

 

#include "GUI.h"

 

 

#include "stdio.h"

#include "stdlib.h"

#include "fsl_ctimer.h"

#include "fsl_sctimer.h"

 

 

#include <stdio.h>

#include "board.h"

#include "peripherals.h"

#include "pin_mux.h"

#include "clock_config.h"

#include <stdio.h>

#include <stdlib.h>

#include <stdbool.h>

#include <string.h>

#include "board.h"

#include "fsl_lcdc.h"

#include "fsl_i2c.h"

#include "fsl_usart.h"

#include "fsl_gpio.h"

#include <cr_section_macros.h>

#include "fsl_iocon.h"

#include "pin_mux.h"

#include "fsl_sctimer.h"

#include "fsl_ctimer.h"

#include "fsl_rtc.h"

#include "peripherals.h"

#include "fsl_DualUart.h"

#include "fsl_sd.h"

#include "fsl_power.h"

#include "fsl_i2s.h"

#include "fsl_codec8814.h"

#include "fsl_dma.h"

#include "fsl_i2s_dma.h"

#include "fsl_enet.h"

#include "fsl_phy.h"

#include "fsl_inputmux.h"

 

#define SDRAM_BASE_ADDR  0xA0000000

#define GUI_BLOCKSIZE    0x128

#define CTIMER CTIMER3

#define VRAM_SIZE  (960000)

static volatile int32_t s_LCDpendingBuffer = -1;

GUI_PID_STATE pid_state;

 

static SemaphoreHandle_t xQueueMutex;

static SemaphoreHandle_t xSemaTxDone;

 

 

 

#include "board.h"

#include "peripherals.h"

#include "fsl_inputmux.h"

#include "pin_mux.h"

#include "clock_config.h"

#include "LPC54618.h"

#include <stdio.h>

#include <stdlib.h>

#include <stdbool.h>

#include <string.h>

#include "board.h"

#include "fsl_lcdc.h"

#include "fsl_i2c.h"

#include "fsl_usart.h"

#include "fsl_gpio.h"

#include "fsl_gint.h"

#include <cr_section_macros.h>

#include "pin_mux.h"

#include "fsl_sctimer.h"

#include "fsl_ctimer.h"

#include "fsl_rtc.h"

#include "fsl_RTC8563.h"

#include "peripherals.h"

#include "fsl_DualUart.h"

#include "fsl_sd.h"

#include "fsl_power.h"

#include "fsl_i2s.h"

#include "fsl_codec8814.h"

#include "fsl_dma.h"

#include "GUI.h"

#include "LCD.h"

#include "WM.h"

#include "stdint.h"

 

 

extern  unsigned char   GuiNumberofBytes[GUI_NUMBYTES];

extern unsigned short V_RamframeBuff[480000];

 

void APP_LCD_IRQHandler(void)

{

    uint32_t intStatus = LCDC_GetEnabledInterruptsPendingStatus(APP_LCD);

 

    LCDC_ClearInterruptsStatus(APP_LCD, intStatus);

 

    if (intStatus & kLCDC_VerticalCompareInterrupt)

    {

        if (s_LCDpendingBuffer >= 0)

        {

            /* Send a confirmation that the given buffer is visible */

            GUI_MULTIBUF_Confirm(s_LCDpendingBuffer);

            s_LCDpendingBuffer = -1;

        }

    }

    __DSB();

}

 

 

 

 

/*******************************************************************************

* Application implemented functions required by emWin library

******************************************************************************/

void LCD_X_Config(void)

{

 

///V_RamframeBuff size  is 960000 bytes  and allocated in external ram

    status_t status;

 

    GUI_MULTIBUF_Config(1);

    if(GUI_DEVICE_CreateAndLink(GUIDRV_LIN_16, GUICC_M565, 0, 0))

    {

    

    }

    else

    {

     

    }

 

    LCD_SetSizeEx(0, 800, 600);

   

 

 

    LCD_SetVSizeEx(0, 800, 600);

 

 

    LCD_SetVRAMAddrEx(0, (void *)V_RamframeBuff);

 

 

    status = APP_LCDC_Init();

 

    if (status != kStatus_Success)

    {

 

    }

 

}

 

int LCD_X_DisplayDriver(unsigned LayerIndex, unsigned Cmd, void *p)

{

       return 0;

}

 

void GUI_X_Config(void)

{

       int i=0,j=0;

       char xyz[10];

 

      ///GuiNumberofBytes size  is 2MB and allocated in external ram

        

 

       GUI_ALLOC_AssignMemory((unsigned char *)GuiNumberofBytes, GUI_NUMBYTES);

    /* Select default font */

    GUI_SetDefaultFont(GUI_FONT_6X8);

    GUI_SetDefaultColor(GUI_BLACK);

    USART_WriteByte(NIBP_USART,'3');USART_WriteByte(NIBP_USART,'4');

}

 

void GUI_X_Init(void)

{

 

}

 

/*********************************************************************

*

*      Multitasking:

*

*                 GUI_X_InitOS()

*                 GUI_X_GetTaskId()

*                 GUI_X_Lock()

*                 GUI_X_Unlock()

*

* Note:

*   The following routines are required only if emWin is used in a

*   true multi task environment, which means you have more than one

*   thread using the emWin API.

*   In this case the

*                       #define GUI_OS  (1)

*  needs to be in GUIConf.h

*/

 

/*! @brief Init OS.Creates the resource semaphore or mutex typically used by GUI_X_Lock() and GUI_X_Unlock().*/

void GUI_X_InitOS(void)

{

       // USART_WriteByte(NIBP_USART,'O');USART_WriteByte(NIBP_USART,'S');

       /* Create a Mutex lock*/

       xQueueMutex = xSemaphoreCreateMutex();

       configASSERT(xQueueMutex !=NULL);

 

       vSemaphoreCreateBinary(xSemaTxDone);

       configASSERT(xSemaTxDone != NULL);

       //USART_WriteByte(NIBP_USART,'1');USART_WriteByte(NIBP_USART,'1');

}

 

/*! @brief Locks the GUI*/

void GUI_X_Lock(void)

{

       //USART_WriteByte(NIBP_USART,'O');USART_WriteByte(NIBP_USART,'S');

       xSemaphoreTake(xQueueMutex , portMAX_DELAY);

       //USART_WriteByte(NIBP_USART,'1');USART_WriteByte(NIBP_USART,'2');

}

 

/*! @brief Unlocks the GUI */

void GUI_X_Unlock(void)

{

       //USART_WriteByte(NIBP_USART,'O');USART_WriteByte(NIBP_USART,'S');

       xSemaphoreGive(xQueueMutex);

       //USART_WriteByte(NIBP_USART,'1');USART_WriteByte(NIBP_USART,'3');

}

 

/*! @brief Get the Task handle */

U32 GUI_X_GetTaskId(void)

{

    return ((uint32_t)xTaskGetCurrentTaskHandle());

}

 

void GUI_X_WaitEvent (void)

{

       //USART_WriteByte(NIBP_USART,'O');USART_WriteByte(NIBP_USART,'S');

       while( xSemaphoreTake(xSemaTxDone, portMAX_DELAY ) != pdTRUE );

       //USART_WriteByte(NIBP_USART,'1');USART_WriteByte(NIBP_USART,'4');

}

 

 

void GUI_X_SignalEvent (void)

{

       //USART_WriteByte(NIBP_USART,'O');USART_WriteByte(NIBP_USART,'S');

       xSemaphoreGive( xSemaTxDone );

       //USART_WriteByte(NIBP_USART,'1');USART_WriteByte(NIBP_USART,'5');

}

void GUI_X_ExecIdle(void)

{

}

 

GUI_TIMER_TIME GUI_X_GetTime(void)

{

       //USART_WriteByte(NIBP_USART,'O');USART_WriteByte(NIBP_USART,'S');

    return ((int) xTaskGetTickCount());

       //USART_WriteByte(NIBP_USART,'1');USART_WriteByte(NIBP_USART,'6');

}

 

/*! @brief Returns after a specified time period in milliseconds. */

void GUI_X_Delay(int ms)

{

       //USART_WriteByte(NIBP_USART,'O');USART_WriteByte(NIBP_USART,'S');

       vTaskDelay(ms);

       //USART_WriteByte(NIBP_USART,'1');USART_WriteByte(NIBP_USART,'7');

}

void *emWin_memcpy(void *pDst, const void *pSrc, long size)

{

    return memcpy(pDst, pSrc, size);

}

status_t APP_LCDC_Init(void)

{

    // Initialize the display.

    lcdc_config_t lcdConfig;

//    lcdc_cursor_config_t cursorConfig;

    LCDC_GetDefaultConfig(&lcdConfig);

    lcdConfig.panelClock_Hz = LCD_PANEL_CLK;

    lcdConfig.ppl = LCD_PPL;

    lcdConfig.hsw = LCD_HSW; //LCD_HSW;

    lcdConfig.hfp = LCD_HFP;

    lcdConfig.hbp = LCD_HBP;

    lcdConfig.lpp = LCD_LPP;

    lcdConfig.vsw = LCD_VSW;

    lcdConfig.vfp = LCD_VFP;

    lcdConfig.vbp = LCD_VBP;

    lcdConfig.polarityFlags = LCD_POL_FLAGS;

    lcdConfig.upperPanelAddr = (unsigned int)V_RamframeBuff;

    lcdConfig.bpp = kLCDC_16BPP565;

    lcdConfig.display = kLCDC_DisplayTFT;

    lcdConfig.swapRedBlue = true;

    lcdConfig.dataFormat = kLCDC_WinCeMode;

    LCDC_Init(APP_LCD, &lcdConfig, LCD_INPUT_CLK_FREQ);

    LCDC_EnableCursor(APP_LCD, false);// LCDC_EnableCursor(APP_LCD, true);

    LCDC_Start(APP_LCD);

    LCDC_PowerUp(APP_LCD);

    return kStatus_Success;

}

we are using 800X600 10.4 inch lcd 

Please help us to resolve the problem

 

IMG_20220725_181829.jpg

Managelinkerscript.pngMemoryDetails.jpgPreProcessors.png

 

Please help us to resolve this issue as soon as possible because I am  already lagging too much on time 

Regards

Nithin N

0 Kudos
Reply