emwin 5.24h floating point

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emwin 5.24h floating point

1,922件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by genesi on Thu Jun 19 05:10:41 MST 2014
Hi there,

Please, can you release emWin 5.24h_fp (floating point) for the keil compiler, as soon as you can? This is important to my application.

Thank you.
Mario
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,875件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jun 23 03:33:42 MST 2014
The Floating point ABIs are described in this FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/cm4-floating-point
0 件の賞賛
返信

1,875件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by genesi on Mon Jun 23 03:20:14 MST 2014
thanks,
what is the differene between Hard ABI and Soft ABI?
that uses the latest version of FP library released 5.24h?
best regards.
Mario
0 件の賞賛
返信

1,875件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sundarapandian on Thu Jun 19 09:30:18 MST 2014
emWin 5.24h M4 library already has floating point enabled.
0 件の賞賛
返信