emWin or Swim

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emWin or Swim

1,491 Views
murugavelan
Contributor I

emWin or Swim

We are using LPC4357 in QFP package and LCD 4.3" with Touch control. emWin or Swim - Which one will be better to use ? Any suggestion some details?

Regards,

Murugavel.A.N

Labels (1)
1 Reply

1,354 Views
brendonslade
NXP TechSupport
NXP TechSupport

SWIM provides a very basic set of drawing primitives plus the ability to display text; it doesnt include any touch screen support. If you want to do anything more sophisticated than that, then emWIN is the way to go. Given your screen size, I would definitely be the best choice. emWIN is also supported in SDK, if/when you want to transition to a new NXP MCU (like LPC546xx or i.mx RT).