emWin library for simulation with mingw/gcc compiler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin library for simulation with mingw/gcc compiler

1,580件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Wed May 20 05:54:49 MST 2015
I'd like to simulate a emWin project on my Windows desktop PC, and I'd like to use mingw/gcc compiler.

Segger usually releases .a pre-compiled library file that can be used during linking process with mingw compiler. It is present in their evaluation version. Now it is available the version 5.26.

The last emWin version released by NXP is 5.24. This release lacks the .a pre-compiler library file, only .lib for Visual Studio.

Is it possible to have .a file too? Now I'm using .a from 5.26 evaluation version, but I don't think it's a good idea.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)