emWin and touchscreen example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emWin and touchscreen example

2,953 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mcresseri on Sat Jul 07 09:38:57 MST 2012
Hi, I'm trying to understand how the touch screen works on the Embedded Artist's LPC1788 developer's kit with the 7" LCD board.
I've loaded on the board the example obtained from segger's website, with the LCD_Conf.c patch from EA's website. I've noticed a problem with the coordinates of the touch screen: when I press a point, the cursor is displayed elsewere.
Also with the "Industrial demo" example I have great problems with the coordinates. In this second example, it is very hard to move the sliders control.
If I use the TOUCH_Calibrate.c example in the sample/tutorial directory of the NXP's emWin 5.14 BSP file, I cannot touch the two points used for the calibration: the touch screen appears unable to detect the pressure of the fingers.
I want to use one of this example as the basis for a "virtual keyboard" application. Have you any suggestion? Any help is greatly appreciated.
Labels (1)
0 Kudos
Reply
1 Reply

1,765 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lien.Nguyen on Sun Jul 08 03:13:50 MST 2012
Hi,
You can try the LCD example in the CMSIS package.
Pls go to http://sw.lpcware.com/?p=lpc177x_8x.git&a=summary.

Best Regards,
Lien
0 Kudos
Reply